Hi,
I am using sabresd iMX6dl with Android 7.1.2, I enabled the watchdog timer in u-boot, There is no booting issue in android level.
Below given the path macro is added
bootable/bootloader/uboot-imx$ git diff include/configs/mx6sabresd.h
#define CONFIG_HW_WATCHDOG
#define CONFIG_IMX_WATCHDOG
But the issue is the watchdog is restating the system every 2mint once .
I don't no what I am missing in kernel and android level configuration.
Please support to fix this issue.
Regards,
Harish
Hi Harish
android is based on linux and one can check if wdog is enabled in kernel using
sect.2.9.2.4 Menu Configuration Options attached Linux Manual.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------