RTC pin external clock requiment in LS1043A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RTC pin external clock requiment in LS1043A

572 Views
ajaykumar_d
Contributor II

I am using LS1043A on my board and want to enable WDOG in my system (custom board) so I need to connect a 32kHz oscillator to RTC Pin and pull down TA_BB_RTC Pin to ground. I am not getting 32kHz oscillator with most of the  Oscillator vendor and do not have any timer device to support lower clock. My system input clock is 100MHZ. is it must to connect only 32kHz or any other clock will work? 

Labels (2)
0 Kudos
1 Reply

430 Views
ufedor
NXP Employee
NXP Employee

In the processor's Data Sheet it is written:

"The minimum period of the RTC signal should be greater than or equal to 16x the period of the platform clock with a 50% duty cycle. There is no minimum RTC frequency"

0 Kudos