Hello I can find the SDK for the LPC1769... when is it going to be available ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hello I can find the SDK for the LPC1769... when is it going to be available ?

3,077 Views
giorgos_h4
Contributor I

I was trying to download the sdk file for the LPC1769 but its not on the website.

1 Reply

2,415 Views
lpcxpresso_supp
NXP Employee
NXP Employee

I'm afraid that there is no MCUXpresso SDK support for the LPC17 family. You need to use LPCOpen instead.

If you are using MCUXpresso IDE, then an appropriateLPCOpen package is included inside the Examples subdirectory of the IDE. See the IDE's User Guide for more details.

For more information on LPCOpen, as well as packages for all toolchains, visit:

Regards,

MCUXpresso IDE Support