About the VSNVS output voltage of PMIC and VDD_SNVS_IN input voltage of i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the VSNVS output voltage of PMIC and VDD_SNVS_IN input voltage of i.MX6

1,496 Views
yuuki
Senior Contributor II

Dear all,

We use i.MX6Solo and PF0100F0AEP.
I seem that a spec of the VSNVS output of PMIC do not match a spec of VDD_SNVS_IN.
I think that the Min value of VSNVS is less than the Min value of VDD_SNVS_IN.

Does this affect the operation of i.MX6solo?
Or, Is it the mistake of specifications of which?


For VDD_SNVS_IN of i.MX6Solo,
According to the "Table 8 Operating Ranges" in Datasheet, it is defined at 2.9V - 3.3V.

Table 8 Operating Ranges.png

However, for VSNVS of PF0100,
According to the "Table 111. VSNVS electrical characteristics" in Datasheet, it is defined in 3.0V +/-5.0%.
So, the voltage range is from 2.85V to 3.15V.

Table 111. VSNVS electrical characteristics.png

May I have an advice?

Best Regards,
Yuuki

Labels (2)
0 Kudos
Reply
1 Reply

1,265 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  The selected in red variant of output PMIC SNVS voltage does not contradict

i.MX6 specs. Also, customers can use the case, based on external coin cell for

the PMIC: 2.84 V < VCOIN < 3.3 V.

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 Kudos
Reply