Can iMX6 act as USB Audio Class 2.0 device?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can iMX6 act as USB Audio Class 2.0 device?

Jump to solution
1,249 Views
stevenlin001
Contributor II

Hi,

I want iMX6 act as a USB audio interface device (Not usb host), but I can't find any information about USB Audio Class in IMX6DQCEC.pdf or IMX6DQRM.pdf. Can iMX6 be configured as USB Audio Class 2.0 device?

thanks,
Steven

Labels (3)
0 Kudos
Reply
1 Solution
923 Views
b36401
NXP Employee
NXP Employee

Both (Linux and Android) BSPs for i.MX6 does support USB Audio.
And also i.MX6 can be configured as USB Audio device. Please look at g_audio module.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
924 Views
b36401
NXP Employee
NXP Employee

Both (Linux and Android) BSPs for i.MX6 does support USB Audio.
And also i.MX6 can be configured as USB Audio device. Please look at g_audio module.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply