I have the fsl-image-mfgtool installed on my T2080RDB-PC. Why every time that I start the T2080RDB-PC I have to configure the network (interface) in Linux? It is normal?
To configure the network I do the following steps:
1) vi / etc / network / interfaces
2) I add the following lines in the interface file:
auto fm1-mac9
iface fm1-mac9 inet static
address 192.168.1.3
net mask 255.255.255.0
3) From the console I execute:
ifup fm1-mac9
Is there any way of not having to configure the network every time I start the operating system?
Hello Sandra Trujillo García,
This is normal, the file /etc/network/interfaces is provided in the package init-ifupdown, you could modify the configuration file in this package and rebuild it into the rootfs.
Please modify the file sources/meta-freescale/recipes-core/init-ifupdown/init-ifupdown/qoriq/interfaces in Yocto, for example:
auto fm1-mac9
iface fm1-mac9 inet static
address 192.168.1.3
net mask 255.255.255.0
Then rebuild package init-ifupdown and regenerate the rootfs filesystem.
$bitbake init-ifupdown -c cleansstate
$bitbake init-ifupdown
$bitbake fsl-image-core
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------