Hello community,
i have some trouble with CodeWarrior and T2081 CPU.
I am trying to valid the DDR with the DDR-configuration (CodeWarrior).
But when i start a DDR-test it failed everytime and the CCS say this:
CCSAPI connection #1 accepted from ELSTJ-W.tq-net.de at Thu Apr 12 11:40:21 2018
check_min_version(serverh=0,*version)
api version: 00000004 00000006
available_connections(serverh=0,*count,*cc)
connections: {0,73,0xa9fee4a5}
cc_version(serverh=0,cc_index=0,index=0,*version)
config_chain(serverh=0,cc=0,count=1,*devlist,*generic)
devlist: t4amp
reset_to_debug(serverh=0,cc=0)
ERROR(39): Subcore error encountered during multicore operation
parse_error_ext(coreh.{serverh=0,cc_index=0,chain_pos=0}, 39)
error: T2080: HRESET occurred during transaction
CCSAPI connection #1 from ELSTJ-W.tq-net.de closed at Thu Apr 12 11:40:22 2018
Can anyone help me please.
Thanks in advance.
Best regards,
Juergen
Hello again,
i think i have the issue fixed. It was some HW issue with HRESET.
But after this i have the next failure with DDR initialization.
"Error configuuring the target! - DDR initialization failed: D_INIT was not cleared by hardware!
Can anyone help me with this.
Thanks in advance.
Best regards,
Juergen