Cant BOOT IMX6 QUAD with Plugin Mode enabled SPL and u-boot.bin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cant BOOT IMX6 QUAD with Plugin Mode enabled SPL and u-boot.bin

832 Views
manojsampathkum
Contributor II

Hi

I have enabled the plugin Mode in u-boot and I am trying to boot QUAD with  SPL and u-boot.bin combination. I am doing for a test case. I flashed those images using MFGTOOLS. When i tried to boot , it is not booting am not getting any log in minicom. But it boots perfectly when i use u-boot.imx instead of SPL and u-boot.bin.

After that i found the fix for  not booting with SPL and u-boot.bin . 

To solve issue in booting SPL  with plugin mode, I am booting it in DDR memory instead of internal SRAM memory.

what is the reason  behind i am not able to boot it in the internal SRAM ??

Is there any restriction  with the plugin mode booting??

Regards

Manoj

Labels (2)
0 Kudos
1 Reply

655 Views
igorpadykov
NXP Employee
NXP Employee

Hi Manoj

reason may be that uboot size is too big for internal SRAM memory,

also this may be posted on uboot mail list:

U-Boot Info Page 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos