Im using a JN5169 with stack JN-SW-4170 build 1735.
The ZED was based on JN-AN-1220 Light Sensor project.
I'm having trouble with the following basic scenario:
* Join ZED to coordinator
* Power down ZED and Coordinator
* Power up ZED
* Allow a rejoin to fail, device goes to sleep
* Power up Coordinator
* Device wakes and attempts rejoin - always fails!!!!
Device wakes and attempts to rejoin epid 00000000000000bb, the log contains following BDB messages:
BDB: Rejoin Cycle 1-A without Disc - on Ch Mask 0x00001000
BDB: ZPS_eAplZdoRejoinNetwork returned a3
BDB: Rejoin Cycle 1-B with Disc on Primary - on Ch Mask 0x00000000
BDB: Rejoin Cycle 1-C with Disc on Secondary - on Ch Mask 0x00001000
BDB: ZPS_eAplZdoRejoinNetwork returned a3
BDB: Rejoin Cycle 2-C with Disc on Secondary - on Ch Mask 0x00001000
BDB: ZPS_eAplZdoRejoinNetwork returned a3
BDB: vNsDiscoverNwk Ch 11 from 0x00001000 BDB_CHANNEL_MAX:26
BDB: vNsDiscoverNwk Ch 11 from 0x00001000 BDB_CHANNEL_MAX:26
BDB: vNsDiscoverNwk Ch 12 from 0x00001000 BDB_CHANNEL_MAX:26
BDB: Disc on Ch 12 from 0x00001000
BDB: APP_vGenCallback [0 10]
BDB: Unscanned channels 00000000
BDB: Ext PAN ID = 0000000000000000
BDB: Channel = 0
BDB: Stack Profile = 0
BDB: Zigbee Version = 0
BDB: Permit Joining = 0
BDB: Router Capacity = 0
BDB: End Device Capacity = 0
BDB: No suitable network! Continue Discovery
BDB: vNsDiscoverNwk Ch 13 from 0x00001000 BDB_CHANNEL_MAX:26
BDB: vNsDiscoverNwk Ch 13 from 0x00001000 BDB_CHANNEL_MAX:26
BDB: vNsDiscoverNwk Ch 14 from 0x00001000 BDB_CHANNEL_MAX:26
BDB: vNsDiscoverNwk Ch 15 from 0x00001000 BDB_CHANNEL_MAX:26
BDB: vNsDiscoverNwk Ch 16 from 0x00001000 BDB_CHANNEL_MAX:26
BDB: vNsDiscoverNwk Ch 17 from 0x00001000 BDB_CHANNEL_MAX:26
BDB: vNsDiscoverNwk Ch 18 from 0x00001000 BDB_CHANNEL_MAX:26
BDB: vNsDiscoverNwk Ch 19 from 0x00001000 BDB_CHANNEL_MAX:26
BDB: vNsDiscoverNwk Ch 20 from 0x00001000 BDB_CHANNEL_MAX:26
BDB: vNsDiscoverNwk Ch 21 from 0x00001000 BDB_CHANNEL_MAX:26
BDB: vNsDiscoverNwk Ch 22 from 0x00001000 BDB_CHANNEL_MAX:26
BDB: vNsDiscoverNwk Ch 23 from 0x00001000 BDB_CHANNEL_MAX:26
BDB: vNsDiscoverNwk Ch 24 from 0x00001000 BDB_CHANNEL_MAX:26
BDB: vNsDiscoverNwk Ch 25 from 0x00001000 BDB_CHANNEL_MAX:26
BDB: vNsDiscoverNwk Ch 26 from 0x00001000 BDB_CHANNEL_MAX:26
BDB BDB_EVENT_NO_NETWORK!
> Device then goes back to sleep.
If I power reset the end device, it joins the coordinator almost right away.
Any help would be greatly appreciated.