A board with i.mx6ul (9*9) and LPDDR2 not work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

A board with i.mx6ul (9*9) and LPDDR2 not work

635 Views
tiantianhuang
Contributor I

I  want to know if the board with i.mx6ul (9*9) and LPDDR2 has been developed, because my board can't run, even the oscillator (24MHz)  dose not work, but the 32.768K has been oscillated.

Labels (1)
0 Kudos
Reply
3 Replies

542 Views
igorpadykov
NXP Employee
NXP Employee

Hi  tiantian

without working 24MHz oscillator processor will not work, for finding problem

please use Hardware Development Guide for the i.MX 6UltraLite Applications Processor
https://www.nxp.com/docs/en/user-guide/IMX6ULLHDG.pdf

also please look at: linux/arch/arm/boot/dts/imx6ul-14x14-lpddr2-arm2.dts

linux-imx.git - i.MX Linux Kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

542 Views
tiantianhuang
Contributor I

Thank you for your reply. As far as you know, Did anyone (or any company) make the development board with i.mx6ul (9*9) and LPDDR2?  Thanks!

0 Kudos
Reply

542 Views
igorpadykov
NXP Employee
NXP Employee

yes such board with i.mx6ul (9*9) and LPDDR2 was developed internally.

Best regards
igor

0 Kudos
Reply