MPC5746C CAN Frozen. Stuck in Frz Mode. DRUN mode fails

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5746C CAN Frozen. Stuck in Frz Mode. DRUN mode fails

1,890 Views
cholland
Contributor V

Hi,

I am not sure what the problem is, but for some reason, I am stuck in FRZ mode.

It might be stuck in 'Stop Mode', since the NOTRDY = 1 and LMPACK = 1. 

I'm not sure if this is related or not, but I can't seem to enter DRUN mode, only RUN0 mode.

We are running on new hardware, So I am led to believe this might be some sort of hardware issue.

Is there any reason, other than hardware, that it would not transition into DRUN mode?

I used the clock initialization example in "MPC574xC_Clock_Calculator_Rev6.xlsm"

The code gets stuck in the while(MC_ME.GS.B.S_MTRANS) loop.

I can transition to mode 4 (RUN0), but it will not transition to mode 3 (DRUN).

I'm not sure if this is directly related to the CAN issue or not?

MC_ME.PCTL[70].R = 1;  /* Might not even need this. All peripherals might be set */
//CAN_0_config_pins(); /* pins aren't needed at this point */
//CAN_FlexCAN_0_config_rx_msg_buffers(); /* Don't need these either */

int i = 0;

/* Module disable */
CAN_0.MCR.B.MDIS = 1;


/* Select Clock */
CAN_0.CTRL1.B.CLKSRC = 0;

/* Module enable */
CAN_0.MCR.B.MDIS = 0;

CAN_0.MCR.B.HALT = 1;
CAN_0.MCR.B.FRZ = 1;

while(0 == CAN_0.MCR.B.FRZACK ){}   /* <----- Stuck */
while(0 == CAN_0.MCR.B.NOTRDY ){}

CAN_0.MCR.B.SOFTRST = 1;
while(1 == CAN_0.MCR.B.SOFTRST == 1){};

This is the SysClk_Init() function. It will successfully transition to mode RUN0, but will not transition to Default DRUN mode.

void SysClk_Init(void)
{

MC_CGM.AC5_SC.R = 0x01000000; //Connect FXOSC to the FMPLL input.

//Set FMPLL to MHz with 16 MHz FXOSC reference.
PLLDIG.PLLDV.R = 0x04010028; //PREDIV = 0, MFD = 40, RFDPHI = 1, RFDPHI1 = 2
PLLDIG.PLLFD.R = 0x00000000; //PLL fractional numerators
PLLDIG.PLLCAL3.R = 0x00004000; //PLL fractional denominator

//Turn on clock sources and select system clock source
MC_ME.DRUN_MC.R = 0x00130172; //Configure DRUN mode settings with sysclk FMPLL_PHI0 (160 MHz).

MC_ME.ME.R = 0;
MC_ME.ME.R = 0x0000A4FD; /* Enable RUN1-3, STOP0, STANDBY0 */
MC_ME.RUN_PC[0].R = 0x000000FE; //Enable peripherals to run in all modes

//Configure the oscillator divided clocks
SIRC.CTL.R = 0x00000011; //SIRC_DIV_CLK is SIRC divided by 1 (0.128 MHz).
FIRC.CTL.R = 0x00000011; //FIRC_DIV_CLK is FIRC divided by 1 (16 MHz).
SXOSC.CTL.B.OSCDIV = 0x00; //SXOSC_DIV_CLK is SXOSC divided by 1 (0.032 MHz).
//FXOSC.CTL.B.OSCDIV = 0x00; //FXOSC_DIV_CLK is FXOSC divided by 1 (16 MHz).

/* Change to RUN0 */
/* write new mode and key */
MC_ME.MCTL.R = 0x40005AF0ul;
/* write new mode and inverted key */
MC_ME.MCTL.R = 0x4000A50Ful;
while(MC_ME.GS.B.S_MTRANS); //Wait for mode transition to complete
while(MC_ME.GS.B.S_CURRENT_MODE != 0x4); //Verify DRUN is the current mode


//Mode transition to DRUN mode:
MC_ME.MCTL.R = 0x30005AF0; //Enter DRUN mode & Key
MC_ME.MCTL.R = 0x3000A50F; //Enter DRUN mode & Inverted Key
while(MC_ME.GS.B.S_MTRANS); //Wait for mode transition to complete
while(MC_ME.GS.B.S_CURRENT_MODE != 0x3); //Verify DRUN is the current mode
}

P.S. I wonder if I need to transition to DRUN mode if the mode is already mode 3?

       Something else seems to not work if I skip the mode switch and just assume its in mode DRUN already.

Thank you,

Labels (1)
5 Replies

1,271 Views
kashambabu459
Contributor I

Hello Mr.Christopher,

We are also facing same problem,

Did you find any solution for this ISSUE?

Note:

We are using Internal Oscillator 16Mhz and FMPll output as 160Mhz

please provide your feedback.

0 Kudos
Reply

1,271 Views
cholland
Contributor V

The development board was using a different XTAL than the Project board.

If your only using 1  board, have to ensure all the clock settings are correct. 

I know it's tough.

Sorry for the late response. Hope you got it working.

0 Kudos
Reply

1,271 Views
martin_kovar
NXP Employee
NXP Employee

Hello Christopher,

could you please share some simple example project, which demonstrates your issue? I will check the project on my side and I will let you know, where is the problem.

Regards,

Martin

1,271 Views
cholland
Contributor V

Hi Martin,

Ok, a little insight.

I am going to fix the DRUN issue before moving to the CAN problem.

I am using the MPC5748G EVB  development board for development, which is using the 40MHz clock.

Our production board is using a 16 MHz clock.

When I set up the Production board clock using the "MPC574xC_Clock_Calculator_Rev6.xlsm", it will fail to enter DRUN mode.

I went back and used the old initialization and at least now, it can transition to DRUN mode.

Perhaps I must not be setting up the clock calculator correctly, or I have to do something else if I am using a 16 MHz external clock?

The old initialization seems to do a lot more than what the clock generator code does, but whatever it does, it seems to work.

The commented SycClk_Init() is the clock calculator that doesn't transition to DRUN mode.

I am using MPC5746C.h Revision 4.0.0

/*----------------------------------------------------------------------------
** Function : MCAL_Mcu_Init
** Description :
** Precondition : Startup executed
** Postcondition: None
** Parameters : None
** Return value : None
**--------------------------------------------------------------------------*/
void MCAL_Mcu_Init(void)
{

/* This method fails to enter DRUN mode */

//SysClk_Init();

/* These are the original initialization routines */
MCAL_Mcu_Config_Pheripheral_Clocks();
MCAL_Mcu_Config_Main_Clocks();
MCAL_Mcu_Config_Modes();
MCAL_Mcu_Set_Mode();
MCAL_Mcu_Config_eMIOS_Clocks();

}

static void MCAL_Mcu_Config_Pheripheral_Clocks(void)
{
/**
* DE = 0 Divider disabled
* DIV = 0
*/
MC_CGM.CLKOUT1_DC.R = 0x00000000ul;

/**
* Clockout1 = 8 FXOSC
*/
MC_CGM.CLKOUT1_SC.R = 0x08000000ul;

/**
* S160 - System Clock / 1 = 64MHz
* DE = 1 enable clock divider
* DIV = 0 divide by (DIV+1)
*/
MC_CGM.SC_DC0.R = 0x80000000ul;

/**
* S80 - System Clock / 1 = 64MHz
* DE = 1 enable clock divider
* DIV = 0 divide by (DIV+1)
*/
MC_CGM.SC_DC1.R = 0x80000000ul;

/**
* S40 - System Clock / 2 = 32MHz
* DE = 1 enable clock divider
* DIV = 1 divide by (DIV+1)
*/
MC_CGM.SC_DC2.R = 0x80010000ul;

/**
* Read Only 0x80030000
* F40 - System Clock / 4 = 16MHz
* DE = 1 enable clock divider
* DIV = 3 divide by (DIV+1)
*/
/*MC_CGM.SC_DC3.R = 0x80030000ul;*/

/**
* Read Only 0x80010000
* F80 - System Clock / 2 = 32MHz
* DE = 1 enable clock divider
* DIV = 1 divide by (DIV+1)
*/
/*MC_CGM.SC_DC4.R = 0x80010000ul;*/

/**
* FS80 - System Clock / 1 = 64MHz
* DE = 1 enable clock divider
* DIV = 7 divide by (DIV+1)
*
* Must be equal to DC1 (MPC5746C ref manual rev 2, 3/2015 p 661)
*
*/
MC_CGM.SC_DC5.B.DIV = MC_CGM.SC_DC1.B.DIV;
MC_CGM.SC_DC5.B.DE = TRUE;

/**
* Read Only 0x80070000
* F20 - System Clock / 8 = 8MHz (F20 clock is fixed at /8)
* DE = 1 enable clock divider
* DIV = 7 divide by (DIV+1)
*/
/*MC_CGM.SC_DC6.R = 0x80070000ul;*/


/**
* Aux Clock 2(ENET0/ENET1) Source Selection
* SELCTL = 0 F40
*/
MC_CGM.AC2_SC.R = 0x00000000ul;

/**
* Read Only
* Aux Clock 3(TRNG) Source Selection
* SELCTL = 0
*/
/*MC_CGM.AC3_SC.R = 0x01000000ul;*/

/**
* Aux Clock 5(PLL) Source Selection
* SELCTL = 1 FXOSC
*/
MC_CGM.AC5_SC.R = 0x01000000ul;

/**
* Aux Clock 6(CLKOUT_0) Source Selection
* SELCTL = 2 PLL
*/
MC_CGM.AC6_SC.R = 0x02000000ul;

/**
* Aux Clock 8(SPI0) Source Selection
* SELCTL = 0 F40
*/
MC_CGM.AC8_SC.R = 0x00000000ul;

/**
* Aux Clock 9(FlexCAN0) Source Selection
* SELCTL = 1 FXOSC
*/
/*MC_CGM.AC9_SC.R = 0x01000000ul;*/
MC_CGM.AC9_SC.R = 0x00000000ul;
}
/*
* PLL should be off when this is called
*/
static void MCAL_Mcu_Config_Main_Clocks(void)
{
/*
* Fast External Oscillator Control Register
*
* OSCBYP = 0 Oscillator Output Used
* OSCM = ?
* EOCV: Don't change micro default value
* M_OSC = 0 Mask Interrupt
* OSCDIV: 0 (divide by 1)
* I_OSC
*/
//FXOSC.CTL.B.OSCBYP = FALSE;
//FXOSC.CTL.B.M_OSC = FALSE;
//FXOSC.CTL.B.OSCDIV = 0u;

/*
* Slow External Oscillator Control Register
*
*/
/*SXOSC.CTL.R = 0x00000000ul;*/

/*
* Slow Internal RC Oscillator (SIRC) Control Register
* DIV = 0 : /1
*/
SIRC.CTL.R = 0x00000000ul;

/*
* Fast Internal Oscillator (FIRC) Control Register
* DIV = 0 Divide by 1
*/
FIRC.CTL.R = 0x00000000ul;

/**
* Its unused but it "must be greater than MFN".
*/
PLLDIG.PLLCAL3.R = 0x09C3C000ul;
/*
* For 16MHz Charger Board
* Fpll = Fvco / (2^(RFDPHI+1))
*
* Fvco = (Fref / PREDIV) * (MFD + (MFN / (MFDEN + 1)))
*
* MFN = 0
* PREDIV = 2 (DIVIDE by 2)
* MFD = 128 (Multiply by 128)
* RFDPHI = 3 (Divide by 16)
* RFDPHI1 = 3 (Divide by 16)
*
* Fvco = (16MHz / 2) * 128
* = 1024MHz
*
* Fpll = 1024MHz / 2^4
* = 64MHz
*/
PLLDIG_PLLDV = 0x06032080ul;

/*
* For 40MHz Charger Board
* Fpll = Fvco / (2^(RFDPHI+1))
*
* Fvco = (Fref / PREDIV) * (MFD + (MFN / (MFDEN + 1)))
*
* MFN = 0
* PREDIV = 5 (DIVIDE by 5)
* MFD = 128 (Multiply by 128)
* RFDPHI = 3 (Divide by 16)
* RFDPHI1 = 3 (Divide by 16)
*
* Fvco = (40MHz / 5) * 128
* = 1024MHz
*
* Fpll = 1024MHz / 2^4
* = 64MHz
*
*/
/*PLLDIG_PLLDV = 0x06035080ul;*/


/**
* DTDHDIS = 1
* MFN = 0;
*/
PLLDIG_PLLFD = 0x00010000ul;

/*
* PLL Modulation Register
*
* SSCGBYP = 1 (Spread Spectrum Modulation is bypassed)
*/
PLLDIG_PLLFM = 0x40000000ul;
}

static void MCAL_Mcu_Config_Modes(void)
{
/* Additionally Enabled Modes: RUN1 (for bootloader until changed) */
MC_ME.ME.R = 0x0000003Dul;

/* Set all used peripherals to use Low Power Config 0 and Run config 0 */
/* PCTL should be configured on AFTER the clocks are configured on.
*
* Also enable RTI timers AFTER these clocks have been configured and activated.
* See clocking overview in 5746C ref manual
*/
/* Set Run Config 0 to be on in all possible modes.
* RUN3, RUN2, RUN1, RUN0, DRUN, SAFE
*/
MC_ME.RUN_PC[0].R = 0x000000FCul;

/* Set Low Power Peripheral Config 0 to be default in all low power modes.
* This means all peripherals that use this config will be off.
*/
MC_ME.LP_PC[0].R = 0x00000000ul;

/* At this point nothing should ever turn off. Thus, no matter the mode we
* will be on external clock with PLL. Hopefully, this does not affect the
* bootloader. It shouldn't since we go there by way of reset.
*/

/*
* Ensure PLL is off. This is the mode after reset. Here we will configure
* the PLL before we switch modes into one operating with the PLL.
*
* PWRLVL = 0 (default)
* PDO = 0 (no auto safe gating)
* MVRON = 1 (main volt reg on) (read only)
* FLAON = 3 (Flash in run mode)
* SXOSCON = 0 (32kHz external osc off)
* SIRCON = 1 (128kHz internal RC osc ON) (used by SWT)
* PLLON = 0
* FXOSCON = 1 (external osc on)
* FIRCON = 1 (16MHz int osc on)
* SYSCLK = 0 (sysclk uses 16MHz internal RC)
*/
MC_ME.DRUN_MC.R = 0x001300B0ul;
/*
* PWRLVL = 0 (default)
* PDO = 0 (no auto safe gating)
* MVRON = 1 (main volt reg on) (read only)
* FLAON = 3 (Flash in run mode)
* SXOSCON = 0 (32kHz external osc off)
* SIRCON = 1 (128kHz internal RC osc ON)
* PLLON = 1
* FXOSCON = 1 (external osc on)
* FIRCON = 1 (16MHz int osc on)
* SYSCLK = 2 (sysclk uses PLL)
*/
MC_ME.RUN_MC[0].R = 0x001300F2ul;
MC_ME.RUN_MC[1].R = 0x001300F2ul;
MC_ME.RUN_MC[2].R = 0x001300F2ul;
MC_ME.RUN_MC[3].R = 0x001300F2ul;
/*
* Stop Mode Default
*
* PWRLVL = 0 (default)
* PDO = 0 (no auto safe gating)
* MVRON = 1 (main volt reg on)
* FLAON = 1 (Flash in power down mode)
* SXOSCON = 0 (32kHz external osc off)
* SIRCON = 0 (128kHz internal RC osc off)
* PLLON = 0
* FXOSCON = 0 (external osc off)
* FIRCON = 1 (16MHz int osc on)
* SYSCLK = 0 (sysclk uses 16MHz internal)
*/
/*MC_ME.STOP_MC.R = 0x00110010ul;*/

/*
* Standby Mode Default
*
* PWRLVL = 0 (default)
* PDO = 1 (auto safe gating)
* MVRON = 0 (main volt reg off)
* FLAON = 1 (Flash in power down mode)
* SXOSCON = 0 (32kHz external osc off)
* SIRCON = 0 (128kHz internal RC osc off)
* PLLON = 0
* FXOSCON = 0 (external osc off)
* FIRCON = 1 (16MHz int osc on)
* SYSCLK = 0 (No System Clock)
*/
/*MC_ME.STANDBY_MC.R = 0x0081001Ful;*/

MC_ME.PCTL[1].B.RUN_CFG = 0x1; /* eMIOS 0: select peri. cfg. RUN_PC[1] */
//MC_ME.PCTL[2].B.RUN_CFG = 0x1; /* eMIOS 1: select peri. cfg. RUN_PC[1] */
}

static void MCAL_Mcu_Set_Mode(void)
{
// MC_ME.MCTL.R = 0xA0005AF0; /* Enter STOP mode and key */
// MC_ME.MCTL.R = 0xA000A50F; /* Enter STOP mode and inverted key */
// while (MC_ME.GS.B.S_MTRANS) {} /* Wait for STOP mode transition to complete */

/* Change to RUN0 */
/* write new mode and key */
MC_ME.MCTL.R = 0x40005AF0ul;
/* write new mode and inverted key */
MC_ME.MCTL.R = 0x4000A50Ful;

/* Wait on transition */
while(MC_ME.GS.B.S_MTRANS);
/* transition automatically waits on FXOSC and PLL Lock if those are on for the mode
* See Clock Sources section 8.9
*/
}
void MCAL_Mcu_Config_eMIOS_Clocks(void)
{
/*
* Generic eMIOS config here.
*
*0 RSVD
*1 MDIS
*2 FRZ
*3 GTBE 1
* 0001
*4 ETB
*5 GPREN 1
*6 NA
*7 NA
* 0100
*8 NA
*9 NA
*10 NA
* 0x0
*11 NA
*12 NA
*13 NA
*14 NA
* 0x0
*15 NA
*16 GPRE
*17 GPRE
*18 GPRE
*19 GPRE
* 0x0
*20 GPRE
*21 GPRE 1
*22 GPRE 1
*23 GPRE 1
* 0x7
*24 NA
*25 NA
*26 NA
*27 NA
* 0x0
*28 NA
*29 NA
*30 NA
*31 NA
* 0x0
*
* MDIS = 0: Clock Running
* FRZ = 0: Do not stop in debug mode
* GTBE = 1: Global Time Base Enabled
* GPREN = 1: Global Prescaler Enabled
* GPRE = 3: Global Prescaler 63 (FS80 / (prescaler +1)
* 64MHz / (7 +1)
* 8MHz
*/
/* eMIOS_0.MCR.B.GTBE = 1; */
/* eMIOS_0.MCR.B.GPREN = 1; */
/* eMIOS_0.MCR.B.GPRE = 0x7; */
/* eMIOS_0_MCR = 0x14000700ul; */
/* eMIOS_1_MCR = 0x14000700ul; */

/* EMIOS 0 Configuration */
eMIOS_0.MCR.B.GPREN = 0; /* Disable global pre-scaler (reset default) */
eMIOS_0.MCR.B.GPRE = 79; /* Divide 80 MHz clock to module by 80 */
eMIOS_0.MCR.B.FRZ = 0; /* No Freeze channel registers in debug mode if channel FREN=0 */

}

//Enable XOSC, PLL0, PLL1, and enter LPU_STANDBY with LPU_SYS_CLK as system clock (160 MHz).
void SysClk_Init(void)
{
MC_CGM.AC5_SC.R = 0x00000000; //Connect FIRC to the FMPLL input.

//Set FMPLL to MHz with 16 MHz FIRC reference.
PLLDIG.PLLDV.R = 0x04010028; //PREDIV = 0, MFD = 40, RFDPHI = 1, RFDPHI1 = 2
PLLDIG.PLLFD.R = 0x00000000; //PLL fractional numerators
PLLDIG.PLLCAL3.R = 0x00004000; //PLL fractional denominator

//Turn on clock sources and select system clock source
MC_ME.DRUN_MC.R = 0x001301F2; //Configure RUN0 mode settings with sysclk FMPLL_PHI0 (160 MHz).
MC_ME.RUN_MC[0].R = 0x001301F2; //Configure RUN0 mode settings with sysclk FMPLL_PHI0 (160 MHz).

//Configure the oscillator divided clocks
SIRC.CTL.R = 0x00000011; //SIRC_DIV_CLK is SIRC divided by 1 (0.128 MHz).
FIRC.CTL.R = 0x00000011; //FIRC_DIV_CLK is FIRC divided by 1 (16 MHz).
SXOSC.CTL.B.OSCDIV = 0x00; //SXOSC_DIV_CLK is SXOSC divided by 1 (0.032 MHz).
//FXOSC.CTL.B.OSCDIV = 0x00; //FXOSC_DIV_CLK is FXOSC divided by 1 (40 MHz).

MC_ME.RUN_PC[0].R = 0x000000FE; //Enable peripherals to run in all modes

//Mode transition to RUN0 mode:
//MC_ME.MCTL.R = 0x40005AF0; //Enter RUN0 mode & Key
//MC_ME.MCTL.R = 0x4000A50F; //Enter RUN0 mode & Inverted Key
//while(MC_ME.GS.B.S_MTRANS); //Wait for mode transition to complete
//while(MC_ME.GS.B.S_CURRENT_MODE != 0x4); //Verify RUN0 is the current mode

MC_ME.MCTL.R = 0x40005AF0; //Enter RUN0 mode & Key
MC_ME.MCTL.R = 0x4000A50F; //Enter RUN0 mode & Inverted Key
while(MC_ME.GS.B.S_MTRANS); //Wait for mode transition to complete
while(MC_ME.GS.B.S_CURRENT_MODE != 0x4); //Verify RUN0 is the current mode
}

0 Kudos
Reply

1,271 Views
cholland
Contributor V

I noticed a difference in the Fpll.

The one that works is using a 64 MHz Fpll (FMPLL_PHI0). 

I tried to setup the (FMPLL_PHI0) for 160 MHz, similar to using the 40 MHz oscillator.

That is one difference I noticed. That and the following 2 Register settings.

    PLLDIG_PLLFD = 0x00010000ul;  /* DTDHDIS = 1 (Dither Disabled) */

    PLLDIG_PLLFM = 0x40000000ul;  /* SSCGBYP = 1 (Spread Spectrum Modulation is bypassed) */

I am not quite sure why those registers are set the way they are?

* Fpll = Fvco / (2^(RFDPHI+1))
*
* Fvco = (Fref / PREDIV) * (MFD + (MFN / (MFDEN + 1)))
*
* MFN = 0
* PREDIV = 2 (DIVIDE by 2)
* MFD = 128 (Multiply by 128)
* RFDPHI = 3 (Divide by 16)
* RFDPHI1 = 3 (Divide by 16)
*
* Fvco = (16MHz / 2) * 128
* = 1024MHz
*
* Fpll = 1024MHz / 2^4
* = 64MHz
*/
PLLDIG_PLLDV = 0x06032080ul;

Thank you,

0 Kudos
Reply