Where can i download the usb driver for IMX6SL device? When connect the PC with USB, it display that EVK_IMX6SL can not find the driver.
computer would install the drvier automatically, if dont detect the board. pls try to connect different usb port of PC,which port are you failed? OTG or UART? I tested OTG successfully, and I open the mfgtool, which can detect the imx6sl board.