How I can install MRF6S27015 model for AWR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How I can install MRF6S27015 model for AWR

1,339 Views
evgenyevgeny
Contributor I

Hello,

I would like to simulate RF power transistor MRF6S27015 in AWR Design Environment, I download "RF High Power Model Kit Rev 4" and try to set model MRF6S27015N_MET, but I can't do it. I made many configuration of xml file via examples for *.mdl files, but It was unsuccessfully. I need help: How I can simulate MRF6S27015 in AWR. I use AWR 13. But I may use others version.

Best regards,

Evgeny

Labels (1)
  • RF

0 Kudos
1 Reply

1,023 Views
andrei_skok
NXP Employee
NXP Employee

NXP doesn't provide MRF6S27015 AWR model, only ADS model.

MRF6S27015N|2300-2700 MHz, 3 W Av., 28 V|NXP 

Please look at the following link for all available AWR models.

Models for NI AWR Corporation Microwave Office®|NXP 

Please note, MRF6S27015N has End of Life status.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos