Hello,
I would like to simulate RF power transistor MRF6S27015 in AWR Design Environment, I download "RF High Power Model Kit Rev 4" and try to set model MRF6S27015N_MET, but I can't do it. I made many configuration of xml file via examples for *.mdl files, but It was unsuccessfully. I need help: How I can simulate MRF6S27015 in AWR. I use AWR 13. But I may use others version.
Best regards,
Evgeny
NXP doesn't provide MRF6S27015 AWR model, only ADS model.
MRF6S27015N|2300-2700 MHz, 3 W Av., 28 V|NXP
Please look at the following link for all available AWR models.
Models for NI AWR Corporation Microwave Office®|NXP
Please note, MRF6S27015N has End of Life status.
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------