Hi,
we are trying to get HDMI display 1366x768 resolution for a HDMI panel which supports only that resolution
Below given link is tried but it dint help much
iMX6 HDMI output 1366x768 resolution
Please help us in getting 1366x768 resolution output from HDMI
BTW we are using imx6q processor and android 7.1.2 version
Hi Harish
HDMI settings on that link was used for another monitor, so
it is necessary to find panel timings in panel datasheet which you are using
and adjust video mode parameters with that specific timings.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------