Hi experts,
I have a following system setup.
HW : Wct-15wtxauto(mwct1013a)
SW : SDK v3.1(WCT_MPTXAUTO_V3.1)
I wonder if the MIN/MAX of Rail Voltage can be controlled by users on the system.
Especially, we want to change the MIN/MAX values depending on the system temperature in real time.
On Freemaster, “Minimum/Maximum Rail Voltage(mv)” are found.
But, the parameters are not used in .c files of SDK. Pls check whether the parameters are used the wct library(It’s a binary file. So we can’t know its internal logic).
Also we found below MACROs in HAL.h. These are used in HAL_SetVrailVoltage( ) API.
#define HAL_VRAIL_MAX_VOL 24000UL
#define HAL_VRAIL_MIN_VOL 3000UL
We guess the function really controls the Rail Voltage.
So the Min/MAX values of Rail Voltage may be applied inside the function if “Minimum/Maximum Rail Voltage(mv)” on freemaster are not used in the wct library.
Pls let me know how the MIN/MAX of Rail voltage can be configured in real-time
BR,
Devin