i.MX6QD flexcan TX signal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6QD flexcan TX signal

717 Views
davideponzetti
Contributor I

Hi, I have a flexcan TX (output) signal doesn't working. I check with multimeter it's connected to the right micro ball but it's programmed as input... with a light 1kohm to gnd the signal fall low as an input pin. At the same time the flexcan RX (input) it seems working good. I can't understand how this is possible. Are there any driver updated or SW tool test for check this item? I'm working on i.MX6 Quad and Dual. Tks, rgds, Davide

Labels (2)
0 Kudos
Reply
1 Reply

607 Views
igorpadykov
NXP Employee
NXP Employee

Hi davide

one can check dts configuration flexcan example in

linux/arch/arm/boot/dts/imx6qdl-sabreauto.dtsi

linux-imx.git - i.MX Linux Kernel 

and test with Demo Images

https://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0_MX6QDLSOLO&appType=license&location=null 

use test procedure in imx-test (../test/can)
www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply