Does any of the MPC56xx (automotive) processors has eFlexPWM to generate high resolution PWM?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does any of the MPC56xx (automotive) processors has eFlexPWM to generate high resolution PWM?

327 Views
rishadahmed
Contributor II

Looking for an AECQ microprocessor to generate high resolution PWM. Regulation window is 200 ns (maximum delay in a phase-shifted full bridge converter). 

Tags (1)
1 Reply

255 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

The MPC5xxx devices offers the FlexPWM module. The fractional delay logic as know e.g. from DSC’s eFlexPWM is not available.

However the FlexPWM clock can be up to 160MHz (on MPC57xx MCUs) so the resolution could be up to 6.25 ns.

BR, Petr