Hi Guys,
We have made a borad which modified from i.MX6UltraLite 14x14 EVK. In ethernet part, the imx6ul's mac is connect to ethernet switch directly (the IC is IP175D link). below is the connection.
The CPU(imx6ul) is connect to the ethernet switch(IP175D) MAC5 using RMII. and make change of uboot (mx6ul_14x14_evk.h) is:
#define IMX_FEC_BASE ENET_BASE_ADDR
#define CONFIG_FEC_MXC_PHYADDR 0x5 /* The IP175D MAC5 mdio address */
#define CONFIG_FEC_XCV_TYPE RMII
When I debug the network using Wireshark with "ping" command, the ARP packet send from imx6, but cpu do not recvice any response. although the response is displayed in Wireshark.
Then I debug the code, and found, all the packet is marked with CRC eror by DMA RxBD:
In driver\net\fec_mxc.c:
if (bd_status & FEC_RBD_ERR)
printf("error frame: 0x%08x 0x%08x\n", addr, bd_status);
where the bd_status is 0x804 and the FEC_RBD_ERR is defined in fec_mxc.h:
#define FEC_RBD_CR 0x0004 /* CRC error */
#define FEC_RBD_ERR (FEC_RBD_LG | FEC_RBD_NO | FEC_RBD_CR | \
FEC_RBD_OV | FEC_RBD_TR)
Then I remove the FEC_RBD_CR bit in FEC_RBD_ERR, and the network is work properly. the packet data is all correct.
Is any reason can let FEC_RBD_CR bit valid? which MAC/PHY parameter is not correct? please help me!
Thanks
Haicheng
Hi Haicheng
seems specific ethernet switch IP175D software (driver) may be used, like
Linux Kernel Driver DataBase: CONFIG_ICPLUS_PHY: Drivers for ICPlus PHYs
for switch configuration one can also look on
configure the ksz8765 5 port Ethernet switch
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------