Dear mohemed aslan,
please check the following tags:
Products | Standard | User memory [bit] | |
---|---|---|---|
ICODE DNA SL2S6002FUD | ISO 18000-3M1 | 2016 | - |
ICODE SLIX 2 SL2S2602 | ISO 18000-3M1 | 2528 | |
ICODE SLIX SL2S2002 / SL2S2102 | ISO 18000-3M1 | 896 | |
ICODE SLIX-L SL2S5002 / SL2S5102 | ISO 18000-3M1 | 256 | |
ICODE SLIX-S SL2S5302 / SL2S5402 | ISO 18000-3M1 | 1280 |
please check this tags all of them have data transfer: up to 53 kbit/s. the most complete of this is the slix S but if you do not need the amount of features please check the slix. in this link you can found the ICODE®|NXP family and you can compare their features.
BR
Jonathan