Hello mario_castaneda,
I am using JN5168-001-M00 Module.
after finishing data transfer from Sleeping Device to Coordinator Successfully.
Now i want to assigned ID for SED(Sleeping End Device).
In multiple SED(Sleeping End Device):
How will i understand that which SED(Sleeping End Device) is sending data to coordinator.
is there any API?
so i can assigned A ID for SED(Sleeping End Device).
I hope you understand my question.
Best Regards,
Dheeraj Sawant
Hi Dheeraj,
I'm sorry, What do you mean with ID for sleep end device?
Do you want to modify the short address assigned by the coordinator?
Regards,
Mario
Hello mario_castaneda,
Did you find any solution for this?
or any available API is Present?
Best Regards,
Dheeraj Sawant
Hi Dheeraj,
You will look for the source address from the message and it will depend on the type of destination, please see the Table 7: Addressing Modes
This structure is used in the ZPS_EVENT_APS_DATA_INDICATION event, which indicates the arrival of data on the local node.
ZPS_tsAfDataIndEvent
https://www.nxp.com/docs/en/user-guide/JN-UG-3101.pdf?fsrch=1&sr=9&pageNum=1
Regards,
Mario
Hello mario_castaneda,
ID means i just wanted to assign a Number to Sleeping End Device.
like example:
if i am having more than 20 sleeping End Device who are sending data to Coordinator. (All are Working)
but i want to find out that which Sleeping End Device is sending data to coordinator.
same thing i want to do.
Hope you understand!
Best Regards,
Dheeaj Sawant