The question says it all
Just to follow up on Jennie's post. There is a debug interface built into the LPCXpresso54608 board that is functionally an LPC-Link2. Alternatively an external debug probe can also be used if required.
Yours,
MCUXpresso Support
The board doesn't show up either as a VSP or any other way. At this point I'm assuming it's defective.
Maybe you can follow this link to update the on-board firmware to see if this can fix the problem, in case the problem is not on the board defective.
https://community.nxp.com/message/925864
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
LPCXpresso 54008 on board debug probe supports CMSIS-DAP/SEGGER J-Link interface.
There is no option to simulate program without a board under MCUXpresso IDE.
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------