Bitdefender marks MCUXpresso IDE as a virus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bitdefender marks MCUXpresso IDE as a virus

3,167 Views
aberger
Contributor V

I am using MCUXpresso IDE v10.1 (and have also checked with v10.0) and Bitdefender Internet Security 2018 on a Windows 10 PC. As soon as I initiate a build, Bitdefender begins quarantining mcuxpressoide.exe (causing the program to exit), and proceeds to quarantine lots of associated files.

Has anyone else experienced this? 

Adding the "\nxp\mcuxpressoide_10.1.0_589" folder to the Bitdefender exclusions list does not solve the problem. I have to completely deactivate Bitdefender in order to build a project in MCUXpresso.

Bitdefender claims that these files contain the "Gen.Atc4.Detection" virus.

0 Kudos
Reply
1 Reply

2,509 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Virus scanning on systems we have here are not showing any such issues (though we aren't using Bitdefender). If your are still seeing problems, I suggest you try again to prevent the scan of the IDE (How to add antivirus exclusions (exceptions) in Bitdefender 2018 ) or report it to them to as a false positive (What to do when Bitdefender detects legitimate applications).

Regards,

MCUXpresso IDE Support

0 Kudos
Reply