More than one TDA8029 in I2C bus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

More than one TDA8029 in I2C bus

823 Views
mariocruz
Contributor I

Hi!

 

 I want to desing a dual contact smart card reader managed by I2c bus. I ´d like to use two TDA8029 ic, but it only has one fixed i2c address. How can I set a different I2c address to one of them for using more than one in parallel?

Thanks a lot!

0 Kudos
Reply
1 Reply

652 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

It only has one fixed I2C address (0x50). Fortunately, it can also be interfaced through RS232. The host interface is chosen by connecting P17 to VDD for RS232 or to GND for I2C.

Please refer to chapter 2.2 Host Controller Interface of the following document:

https://www.nxp.com/docs/en/application-note/AN10207.pdf

 

I hope this helps.

 

Regards,

Ivan.

0 Kudos
Reply