Hi
I'm confusing recommended external cap value for LICELL pin because there are vary as following.
https://www.nxp.com/docs/en/data-sheet/PF3001.pdf
p9 Coin cell supply input/output. Bypass with 0.1 μF capacitor. Connect to optional coin cell.p40 Coin cell battery backup
A 0.47 μF capacitor should be placed from LICELL to ground under all circumstances.p41 Table 57. Coin cell charger external components
LICELL bypass capacitor 100 nFp79 Figure 26. Typical application schematic
220nF
I guess the value in p9,p41 and p79 for the cap with coin cell and the value in p40 for the cap (with or) without coin cell.
Now I think there is no issue to eliminate coin cell like following.
https://community.nxp.com/message/819606
Which one recommended 0.1uF or 0.47uF for the cap of LICELL pin without coin cell?
Can anyone help me?
已解决! 转到解答。
Typically, a 100nF capacitor should be used with the connected coincell, and 0.47uF one - without a coincell.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Typically, a 100nF capacitor should be used with the connected coincell, and 0.47uF one - without a coincell.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------