video live streaming with IMX6ULL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

video live streaming with IMX6ULL

2,525 Views
jomsabu
Contributor I

We have a project based on the camera. The camera module will provide its output as CVBS(Composite Video) and a decoder IC is used to convert the analog signal to parallel.
We need to live streaming the captured video to any local WiFi device.

Our concept is below,

  • Processor: i.MX6ULL.
  • Decoder: TVP5150AM1.
  • WiFi : ISM43362-B81.

Queries:

  • Is it possible to interface the processor i.MX6ULL with decoder TVP5150AM1?
  • Can we compress the image with I.MX6ULL and is it possible to live streaming the captured video to local WiFi device?
0 Kudos
Reply
3 Replies

1,636 Views
jomsabu
Contributor I

Hi,

Thank you to team for the support.

Regard

Jom Sabu

0 Kudos
Reply

1,636 Views
joanxie
NXP TechSupport
NXP TechSupport

for tvp5150,pls refer to the enclosed appication note

1,636 Views
ramyaravichandr
Contributor I

Hi Jom Sabu,

From the following link, there is no specific interface for connecting decoder

i.MX 6UltraLite Applications Processor|NXP 

Please refer the below link, for iMX decoder support.

V4L, iMX6 and TVP5150 

Thanks,

Ramya

www.blackpeppertech.com

0 Kudos
Reply