The question I've meet is that I used the TWR-56F8400 board's OSBDM to download the program to my MC56F84789 chip,but it's alaways failed. When I cut the main circuit'sinta power and only link the TWR_56F8400's USB port to my computer,link the TWR-56F8400's JTAG port to the main circuit's JTAG port , the code can be downloaded to the main circuit 'MC56F84789 chip .However,when I turn on the main circuit's power.It's always failed to download.The CodeWarrior's intarface shows that the chip is secured. When I click the "yes" button,It shows…….
When I click the retry,it still don't work and popup the same window.
It really bother me a lot.I'm looking forward to your help.
Best Regards,
Yong Yan
Hi Yong.
This is the same question as
https://community.nxp.com/message/943622
Please refer above link for answer. Thanks.
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------