Hi,
I have a custom BLE GATT profile working with BlueZ and can R/W characteristic values over BLE from a mobile phone etc. The difficulty I'm having is finding information on how to get access to the characteristic data on board my imx7s platform. The BLE profile will set-up various product functionality and be a general user tool. For example if the user wants to change the host name, set a LED, add another WIFI user to wpa_supplicant and so forth. So as mentioned, I can change the data via a phone, but how do I tap into Bluez and access the data from another application also running on the same Linux OS?
[ Phone ] App ( sets LED characteristic to on ) ================> [imx7s] HCI => Bluez => Custom Profile => BlueZ < == ?? How => C application that sets the LED to on.
The ??How is the mystery. Can I access and R/W my custom Profile's GATT characteristic via D-Bus for similar?
Regards,
Edward
Solved! Go to Solution.
Modified version example-gatt-server gave all the back0end hooks.