Hi, I got the NXP T2080RDB-PC, I want to download C or C++ on it . How can it be done?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi, I got the NXP T2080RDB-PC, I want to download C or C++ on it . How can it be done?

445 Views
natisteinmetz
Contributor I

Hi, I got the NXP T2080RDB-PC, I want to download C or C++ on it . How can it be done?

0 Kudos
2 Replies

349 Views
Pavel
NXP Employee
NXP Employee

NXP offers SDK Linux BSP for the T2080. This SDK provides toolchain for the T2080. This toolchain provides developing application on C and C++. This toolchain is work on the PC.

Look at the following page about building a toolchain on your own board:

http://elinux.org/Toolchains


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

349 Views
natisteinmetz
Contributor I

thanks for the rapid reply.

can you tell me how i can acquire the BSP you mention?

tnx,

nati

0 Kudos