HELLO,everyone, I want add a Flash Devices to the EPPC Flash Programmer .but i don't know how to Generate a Flash Entry for the Master Configuration File Using a Perl Script,following is the method in datasheet.
"Run the script.
At the command line, type:
perl flash_entrygen.pl > “device_name.txt”
Perl should be in the system path. After the script finishes successfully, the device_name.txt file will contain a Flash
entry to add to FPDeviceConfig.xml."
i couldn't find the command-line and how to use the script,please help me
Look at attached file. It is documentation from CodeWarrior 8.8 folder. Use the following path: C:\Program Files (x86)\Freescale\CodeWarrior PA V8.8\PowerPC_EABI_Tools\FlashProgrammer
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yu Tian.
What's your chip part number? Please let me know thus we can contact a proper engineer to check your issue.
Thanks.
Jennie Zhang
my cpu is MPC8555,flash is W78M32V70BM,software environment is codewarrior v8.8,i could not find the similar flash in flash programmer tool,so i need to add a new flash to flash programmer tool,but i don't know how to generate a Flash Entry for the Master Configuration File Using a Perl Script,please tell me the details about the methods,thank you very much!