Hi,
In SDK 2.0, QE firmware (iram_Type_A_LS1021a_r1.0.bin) is not loaded in ls1043ardb when booting from sd card. But this QE firmware is loaded when booting from nor flash. My concern is what will happen if QE firmware not loaded?
If QE microcode is not loader, the LS1043a QE is not work.
NXP SDK 2.0-1703 provides QE microcode loading only from NOR Flash. See u-boot.cfg file in the attachment. This file is available in the folder "ls1043ardb_sdcard_config" in u-boot source folder.
Find the CONFIG_SYS_QE_FW_ADDR in this file.
The simplest way for loading QE microcode from SD card is the following:
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------