I have a prototype with PN7120. I have to detect a falling RFID tag. So how can I enable continuous scanning with a permanent enabled RF field? My first tests with CLRC66302HN has been working really well. But now, I have to adopt the PN7102. How can I configure that chip? My prototype is based on an raspberry 3.
The actual polling time of about 500ms is much too long.
Hi,
PN7120's polling loop consists Listening phase and Polling phase, we may program the duration of Listening phase, but polling phase has fixed time depending on the profile you select. To configure the listen mode, use the following parameter.
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------