I have a CSMB-12XDT512 and since I have a 64 bit computer I cant get it to debug on with FreeScale V5.1 software with just a USB cable that I could once do with windows 32 bit and I know you have to use a USB BDM Pod but the 6 pin BDM on my board has no pins, am I supposed to solder some on it? Has someone already had this problem and did it work?
Hi,
Yes, unfortunately, TBDML interface drivers are not supported on 64bit OS.
You can use the BDM interface, for instance P&E USB Multilink, you will need to mount the BDM port.
Or you can use a virtual 32bit PC, as it is explained in AN3936.
Regards,
Daniel