Developement environment SPC5607BF1MLU6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Developement environment SPC5607BF1MLU6

875 Views
stefanschiebel
Contributor II

Hello,

I have two questions for programming an processor (SPC5607BF1MLU6):

-Can you recommend an developement environment (with an included compiler and linker) for these processor (spc5607BF1MLU6)?

-If I order the evaluation board, is it possible, to get one or two sample processors for testing?


Thank you in advance for your reply.

0 Kudos
Reply
2 Replies

753 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

1) I can recommend you S32 Design Studio, which is free for use.

S32 Design Studio IDE|NXP 

2) I am not sure, but I think the answer is no. You must order microcontrollers separately.

Regards,

Martin

0 Kudos
Reply

753 Views
stefanschiebel
Contributor II

Hello,

can somebody help me with that topic?

Thanks

Stefan Schiebel

Porsche Engineering Services GmbH

0 Kudos
Reply