Hello,
I want use MC33908 for 24v System, but I found its green operation voltage range was 6.0~28V. The max voltage in 24V system may higher than 28V. In datasheet it is said between 28V~40V " Potential Vpre thermal limitation". What will MC33908 works between 28V to 40V? If my load is not high, can I use it in 24V system?
Hello,
Our proposal for 24V systems, as shown in Figure 31 of AN4766, is to insert a Maxim device MAX6495 between Vbat and Vsup to protect the input voltage of MC33908, plus other local protections on pins going or coming from outside of the module.
Best regards,
Tomas