Hi,
I used Codewarrior 10.7.
I use KEA32 but the program can not be downloaded.
Downloading binary to target...
I know that the header file is wrong and I have tried it with other KEA series header files.
Help me...
Hi,
Thank you for your reply.
I am using KEA32 as a 32pin. Making PCB
When I download the program, I get up to 100%, but 'downloading binary to target ...'
I don't know that...
Hi CheolMin Lee
Could you describe more what is the error that you get when you try to download the binary. What do you mean with I have tried it with other KEA series header files.?
You shouldn't change the header file that code warrior generate when you create the project, so please describe more your issue.
Best Regards
Jorge Alcala
Hi
I believe that S32 Design Studio is what tends to be used with the KEA32 - I don't know that CW10.7 supports programming and debugging it(?)
Try a binary from here in case you think it may be a problem with the binary being used: http://www.utasker.com/kinetis/FRDM-KEAZN32Q64.html
Regards
Mark