MPC5744 Debug error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5744 Debug error

2,794 Views
dsytj88
Contributor II

Version:S32 v1.2

after flashing the file into MCU.I tried to use debug mode to lauch MPC5744P.elf file,

in the progress it will be blocked,and error box appeared:

Error with command: gdb --version
Cannot run program "gdb": Launching failed

I tried another demo and it shows the same problem,do you know what's the reason and how to resolve it?

thank you

Labels (1)
0 Kudos
Reply
1 Reply

2,272 Views
stanish
NXP Employee
NXP Employee

Hi,

Could you possibly check if the debug configuration is complete.

pastedImage_1.png

I'd also recommend you to try to create a new workspace in  v1.2 and import your project.

Hope it helps.

Stan 

0 Kudos
Reply