NFC-explore with ISO 14443 Type B Compatibility

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC-explore with ISO 14443 Type B Compatibility

1,466 Views
manojrohitvempa
Contributor II

Hello guys,

 

I have downloaded the NFC Reader Library from http://www.nxp.com/pages/:NFC-READER-LIBRARY. I downloaded the previous Version "NFC Reader Library for Linux" version 4.040.05.011646". Because the latest library for Linux is not compatible with explore-NFC board.

 

I was able to detect Type 4B tag as I was able to obtain the UID. But I am not able to obtain the Ndef message.

When I run the 'NfcrdlibEx3_NFCForum' I was able to detect the NDEF message for Mifare Cards. But not for Type 4B tags. Is there any example I am missing which can read NDEF Messages with explore-nfc.

 

Thank you in advance. 

Labels (2)
0 Kudos
Reply
1 Reply

1,018 Views
jimmychan
NXP TechSupport
NXP TechSupport

we don't have an example showing how to use NDEF messages on the TypeB, our focus is on Type A, MIFARE cards.
To be able to write an NDEF message, I would suggest looking at TypeB specifications.

0 Kudos
Reply