FLASH_DRV_ReadResource(const flash_ssd_config_t * pSSDConfig,
uint32_t dest,
uint8_t * pDataArray,
uint8_t resourceSelectCode)
the function is in s32ds'demo of flash.
I want to read flash data, which function I can use;
Hi,
I cannot find the FLASH_DRV_ReadResource() function somehow.
Nevertheless, to read Flash you can simply use a pointer to the address you can read
data = *(unsigned int*)address;
or use DMA or use memcpy function (string.h)
memcpy(&destination, &source, number_of_bytes)
Regards,
Daniel