HI ,
I want to flash my target board having SDcard using MFGtool . I downloaded the MFgtool L4.1.15_2.0.0-ga_mfg-tools from NXP site. This packages has two folders mfgtools-with-rootfs and mfgtools-without-rootfs . My questions are as follows :-
1. Both the folders having MFGtool.exe , so what's the difference is these two.
2. Can I use this package for flashing the IMX6 based target board .
Please suggest.
Regards,
Aditya Nagal
Hi Aditya,
What board are you using?
Please note that MFGtool was developed to be used with our evaluation boards. If you want to use MFGtool with a custom board you need to build an image that Yocto provides with all the settings to be used with MFGtool and edit it with you ddr settings.
Please find below some discussions and documents about this:
MFGTool for custom i.MX6SL board
i.MX6 DDR Stress Test Tool V1.0.3
Best regards,
Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------