which is the fastest speed for boot from imx6 solo,emmc-spi nor falsh-nan flash?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

which is the fastest speed for boot from imx6 solo,emmc-spi nor falsh-nan flash?

1,101 Views
翔李
Contributor IV

HI,

which is the fastest speed for boot from imx6 solo,emmc-spi nor falsh-nan flash?

And,what about the write speed?

I read the spec. of them a long time,but still not find the speed of read and write,except emmc.

thanks.

emmc:THGBMDG5D1LBAIL

spi nor flash:W25Q256FVEIG

nand flash:W29N02GVSIAA

pastedImage_1.png

pastedImage_2.png

pastedImage_3.png

pastedImage_4.png

0 Kudos
Reply
1 Reply

768 Views
art
NXP Employee
NXP Employee

The fastest boot media of the ones you've specified is eMMC by Toshiba.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply