Now, I'm using P1010 with EHCI controller under VxWorks 6.9.46.
Due to USB issue, I'm wondering if it's possible to force P1010 to be in USB 1.1 configuration using UHCI or OHCI controller ?
Thanks in advance for your reply,
Regards,
Fabrice DECROP
Add 1.5k resistor from the D+ line to USB_VBUS
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Add 1.5k pull-up resistor on the D+ line.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
To what voltage is the pull-up resistor ?
Thanks in advance,
Regards,
Fabrice DECROP
You can also add an external resistor for disabling high-speed mode.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Could please tell me wich resistor is it ?
Thanks in advance,
Regards,
Fabrice DECROP
The P1010 USB hardware can be used to support for connection only in full-speed mode. See the PORTSC[PFSC[ field.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------