Hello,
I have custom board. It has two decoders for two different cameras. I need to configure their simultaneous work.
Standart
adv7280: adv7280@20 {
compatible = "adv7280";
reg = <0x20>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_ipu1_csi0>;
clocks = <&clks 200>;
clock-names = "csi_mclk";
DOVDD-supply = <®_3p3v>;
AVDD-supply = <®_3p3v>;
DVDD-supply = <®_3p3v>;
PVDD-supply = <®_3p3v>;
csi_id = <1>;
mclk = <24000000>;
mclk_source = <0>;
status = "okay";
};
v4l2_cap_0 {
compatible = "fsl,imx6q-v4l2-capture";
ipu_id = <0>;
csi_id = <1>;
mclk_source = <0>;
status = "okay";
};
pinctrl_ipu1_csi0: ipu1grp-csi0 {
fsl,pins = <
MX6QDL_PAD_EIM_A17__IPU1_CSI1_DATA12 0xb0b1
MX6QDL_PAD_EIM_A18__IPU1_CSI1_DATA13 0xb0b1
MX6QDL_PAD_EIM_A19__IPU1_CSI1_DATA14 0xb0b1
MX6QDL_PAD_EIM_A20__IPU1_CSI1_DATA15 0xb0b1
MX6QDL_PAD_EIM_A21__IPU1_CSI1_DATA16 0xb0b1
MX6QDL_PAD_EIM_A22__IPU1_CSI1_DATA17 0xb0b1
MX6QDL_PAD_EIM_A23__IPU1_CSI1_DATA18 0xb0b1
MX6QDL_PAD_EIM_A24__IPU1_CSI1_DATA19 0xb0b1
MX6QDL_PAD_EIM_D17__IPU1_CSI1_PIXCLK 0xb0b1
MX6QDL_PAD_EIM_EB3__IPU1_CSI1_HSYNC 0xb0b1
MX6QDL_PAD_EIM_D29__IPU1_CSI1_VSYNC 0xb0b1
>;
};
Custom
adv7280_1: adv7280@21 {
compatible = "adv7280";
reg = <0x21>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_ipu1_csi1>;
clocks = <&clks 200>;
clock-names = "csi_mclk";
DOVDD-supply = <®_3p3v>;
AVDD-supply = <®_3p3v>;
DVDD-supply = <®_3p3v>;
PVDD-supply = <®_3p3v>;
csi_id = <0>;
mclk = <24000000>;
mclk_source = <0>;
status = "okay";
};
v4l2_cap_1 {
compatible = "fsl,imx6q-v4l2-capture";
ipu_id = <0>;
csi_id = <0>;
mclk_source = <0>;
status = "okay";
};
pinctrl_ipu1_csi1: ipu1grp-csi1 { // parallel camera
fsl,pins = <
MX6QDL_PAD_CSI0_DAT12__IPU1_CSI0_DATA12 0xb0b1
MX6QDL_PAD_CSI0_DAT13__IPU1_CSI0_DATA13 0xb0b1
MX6QDL_PAD_CSI0_DAT14__IPU1_CSI0_DATA14 0xb0b1
MX6QDL_PAD_CSI0_DAT15__IPU1_CSI0_DATA15 0xb0b1
MX6QDL_PAD_CSI0_DAT16__IPU1_CSI0_DATA16 0xb0b1
MX6QDL_PAD_CSI0_DAT17__IPU1_CSI0_DATA17 0xb0b1
MX6QDL_PAD_CSI0_DAT18__IPU1_CSI0_DATA18 0xb0b1
MX6QDL_PAD_CSI0_DAT19__IPU1_CSI0_DATA19 0xb0b1
MX6QDL_PAD_CSI0_PIXCLK__IPU1_CSI0_PIXCLK 0xb0b1
MX6QDL_PAD_CSI0_MCLK__IPU1_CSI0_HSYNC 0xb0b1
MX6QDL_PAD_CSI0_VSYNC__IPU1_CSI0_VSYNC 0xb0b1
>;
};
But together they do not want to work. Although individually everything works. What did I do wrong?
Hi Valentin
unfortunately I am not familiar with this board, seems it is necessary to appropriately
configure VC (virtual channels), please check examples on
https://community.freescale.com/docs/DOC-328548
two camera work at the same time
https://community.nxp.com/message/433706?commentID=433706#comment-433706
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------