What is the function of the DP_GWSEL bit?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the function of the DP_GWSEL bit?

496 Views
richogrady
Contributor II

The imxs6dlrm manual (04/2015) is not clear on this function.  On page 2932 it says:

   "The DP_GWSEL bit defines if the BG is the pixel coming from the full plane or the partial plane."

On page 3269 it says:

   "GWSEL - Graphic Window Select"
   "Select graphic window to be on partial plane or full plane."

Please clarify.

Labels (2)
0 Kudos
Reply
2 Replies

445 Views
richogrady
Contributor II

Thanks.  So "graphic window" means BG (background plane)?

0 Kudos
Reply

445 Views
joanxie
NXP TechSupport
NXP TechSupport

DP_GWSEL bit determins which plane used for graphic window, when DP_GWSEL=0, dev/fb0(full plane) is used for BG, this is default in BSP, when DP_GWSEL=1, dev/fb1(partial plane) is used for BG.

0 Kudos
Reply