I want to use FXTH871X7 for Tyre pressure measurement but the evaluation board is not available. is there any alternative solution for evaluation board (TPMS870911 evaluation board). plz suggest
Hello Chitra,
Thank you for your interest in NXP TPMS devices.
Unfortunately I am not really sure what part and EVB you are looking for.
Part numbers of the FXTH indicated on the datasheet are the following:
FXTH8705xx for 450kPa;
FXTH8709xx for 900kPa;
FXTH8715xx for 1500kPa.
Then xx can refer to:
02 for the standard 1-axis device (e.g. FXTH870902 for 900kPa 1-axis);
11 for the standard 2-axis device;
12 or 22 for non-standard versions.
So please let me know which part you are interested in and I will recommend a suitable EVB.
Best regards,
Tomas
Hello Thomas,
Thank you for your reply.
But for my TPMS chip FXTH871x7, part no. is F875B11XACFA and it is a 2-axis device for 1500kPa. So I am not aware what type of EVB or development board I can use for programming the chip.
Please suggest me the appropriate development board and EVB for programming the TPMS chip FXTH871x7.
With Regards,
Chitra Gautam