Sorry, vxWorks OS is proprietary OS, and supported solely by its vendor - WindRiver corporation.
We do not have any experience with this OS here, in NXP online technical support, so I can not comment regarding proper address to burn vxWorks code and etc vxWorks-related questions.
Regarding 5W 200 Ohm resistor - I do not see this resistor in board BOM, could you please submit its reference designator number or photo?
Have a great day,
Alexander
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Alexander –
Is there any possibility we can exchange the Rev.C board for a rev B ? Also, I heard from Windriver that the big difference between Rev B and C may be the RCW file but I don’t have a copy
for the RCW file for RevB equivalent to the vxWorks7 file T2080RDB_RRFFXXP_66_15_1800MHz.bin. Can I get that file from you?
thank
Frank
Clarification regarding 5W resistor - we have 5W 22 Ohm resistor connected directly at ATX power supply connector, this resistor is used as load for 5V power supply output of ATX power supply, this is necessary for several power supplies to improve power supply stability. If this resistor is disconnected by one end in your case than please connect it between ground (black wire) and +5V (red wire).