K82 - how to use RTC to wake up from VLLSx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K82 - how to use RTC to wake up from VLLSx

583 Views
niranjan_rao
Contributor II

Hello,

I am working with K82 (SDK-2.1). 

I am able to switch between different power-modes and use external pin a to wake up from VLLS0.

I am looking for an example how to wake-up from VLLSx mode using the RTC alarm.

I wan not able to find one, can someone help me with this please?

cheers

Rao

Labels (1)
Tags (3)
2 Replies

414 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Using RTC module is quite similar with using LPTMR module to wake up the core from low power mode.

There with the demo (power_manager or power_mode_switch of KSDK software) to using LPTMR to wake up the core from VLLSx low power mode.

Please check attached K60 RTC wake up the core from LLS low power mode bare-metal project software  for your reference.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

414 Views
niranjan_rao
Contributor II

Hello Ma Hui,
Thank you for the example project, it helped me understand how to initialize the LLWU (RTC)

0 Kudos