Hi~
It is very simple question!!
How to do autologin in yocto?
Best regards,
Colin Park
set_image_autologin()
which looks in /etc/sysconfig/gpelogin
for a variable AUTOLOGIN, but let me remind, if you use the image core-image-sato which doesn't support autologin. I find a link is useful for you, pls refer to it.
<http://stackoverflow.com/questions/28341038/autologin-for-ubuntu-yocto-image>.
Thank you for your feedback.
I am using the image core-image-base. Is it supported autologin??
Reg: Auto-Login and run a script Automatically
you can try this solution, or you can do something similar using the ROOTFS_POSTPROCESS_COMMAND[1] to
change the login manager configuration file to enable autologin.
for image, suggest to use the image you own build. but you can try the solution above first.