Imx6q how to add CAN2 (flexcan1)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Imx6q how to add CAN2 (flexcan1)

777 Views
李鹏斌
Contributor II

Imx6q how to add the second CAN (flexcan1), the STBY of the second CAN pin which is it?

Labels (1)
0 Kudos
Reply
2 Replies

677 Views
igorpadykov
NXP Employee
NXP Employee

Hi

please use imx6q-sabreauto-flexcan1.dts

linux-imx.git - i.MX Linux Kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

677 Views
李鹏斌
Contributor II

Thank you for your reply, I use the version is "linux3.0.35", I would like to use the "kernel imx6q_add_flexcan1" to add the second CAN, but I do not know how to define "mx6q_sabresd_flexcan1_pdata",

"Mx6q_sabresd_flexcan1_pdata" is defined as follows:

can.png

0 Kudos
Reply