Software package for NT3H1101/NT3H1201!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Software package for NT3H1101/NT3H1201!

877 Views
oliverkuo
Contributor IV

Hello NXP's member,

Do you have any software package of NT3H1101 that implements NFC Host-based Card Emulation for Android 6.0.1-2.1.0 BSP?

Or documents describe how to enable Android 6.0.1 HCE support and adapt to other NTAG solution.

Platform: i.MX6Q custom board

NFC Interface: I2C

BSP: android_M6.0.1_2.1.0

Thanks in advance.

Oliver

Labels (3)
0 Kudos
2 Replies

527 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Oliver,

    Our android BSP for I.MX6 series SoC doesn't support NFC by default, If you need to use them, you refer to the link:

http://www.nxp.com/documents/application_note/AN11597.pdf  ( NTAG I²C demo application for Android )

Other documents are here :

NT3H1101/NT3H1201|NXP 

Best Regards,

Weidong

0 Kudos

527 Views
oliverkuo
Contributor IV

Hi Wigros,

   Thanks for your feedback, seems the documents of NT3H1101/1201 you provided are not implemented on Android side.

Whether the Android only implements NFC controller for full NFC function,no NTAG and HCE only?

BTW, may I have the software package of NXP's PN7xx/PN5xx for Android 6, is it opened?

As I know, lots of mobile devices have NXP's NFC solution inside!

Best regards,

Oliver

0 Kudos